Hi,
this is regarding the buck converter TPS54526PWPR. We are using the schematic generated by Web bench for input voltage of +12V and output of 1.2V / 5A.
In this schematic, pin 11 (SW1) is not connected and pin 8 and 9 are not short to ground. But the schematic in the datasheet shows these pins connected.
Please clarify if the pin 11 is to be connected to pin 10 or can it be left open.
Thanks,
Elizabeth