This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2C driver for 2 digit 7-segment LED?

Other Parts Discussed in Thread: LM3463, TPS92660I need to drive a remote 2 digit 7-segment LED from a micro controller with as few leads as possible (it is about 3m from the micro) I figured I2C would be best. Ideally the driver would use the local 12V power source (11V to 14.4V) but accept I2C data at 5V. Do TI make such a driver?