This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fuel Tank BoosterPack not working



Hi,

 I was wondering if anyone had an experience with BOOSXL-BATTPACK.

I've got one to test it, but couldn't make it to work.

I left the battery to be charge and it never indicates the end of charge. Battery voltage ~4.1V with no load

Then I left if running with Tiva Launchpad for a few hours. The battery went low, battery voltage ~3.6V with no load.

After that it doesn't charge the battery, only indicates battery low.

After connecting to another charger battery starts charging.

What is the trick with that board?

Jan