This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need Vbus USB signal switch for TUSB1210?

Other Parts Discussed in Thread: TUSB1210

Team,

We have the TUSB1210 questions answered with the exception of #2.  I am including all for your reference.

1.  We plan onusing this in both Host and Device Mode.  We have been struggling with how
to hook up the CPEN and Vbus signals to support both modes.  My assumption
would be Figure 10-1 would cover both options where as Figure 10-2 is a Device only
mode.   << ANSWERED>>

2.  Do you havea suggestion for a Vbus switch to use with this component.  There are
quite a few on TI, and it was not obvious what would be the best solution.
Our driving requirement is cost and -40 to 105C temp range.  We also
need lead-free.

3.  Per Figure 5-1, it shows that Vdd33 (3.3V) should come up before Vdd18 (1.8V).
However, no additional information is provided on the requirements for
that power sequencing.  We have an issue on our board in which all of our
other multi-voltage devices require 1.8V to come up before or at the same time
as 3.3V.  What would be the implications of bringing up 1.8 before 3.3 or
at the same time?  <<ANSWERED>>

Please point us in the direction of a good Vbus switch.   

 

Thanks,

Aaron