This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Searching PMU (I can't find the some datasheet of PMU)

Guru 20090 points
Other Parts Discussed in Thread: LP3923, TPS65023, TPS650250

Hello,
 
I'm searching PMU which have below function from our customer request.
I can't  find detail of the PMU due to there is no datasheet on the web.
Please kindly help us...
LP3923 is close to our customer request.
However , we can't change the device default voltage.  
 
Are there any device which has below outputs?
----- 
<9 LDOs>
1.5V 200mA
1.8V 200mA
3.0V 200mA 
3.0V 200mA
3.0V 200mA
3.3V 700mA
3.3V 200mA
3.0V 200mA
3.0V 200mA
 
PMU must ouput these device as default value.
<Charger>
1cell Li-ion
 
Not decided specification yet.
----- 
 
Best Regards,
Ryuji Asaka