This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fusion Not Reporting GPOs on UCD9090

The report tool of the Fusion Digital Designer reports how all the rails are configured.  (It is not easy to read because it is a wide spreadsheet so all the parameters of one rail cannot be seen at once.  Maybe a vertical format of each rail would be better.)

However, the GPOs do not show up in the report, and I do not see a way to get a report of how the GPOs are configured.  The only way I see is to copy them down by hand which is tedious and error prone.  Is there a way to get a report of the GPO configuration?

  • The report is a summary of sequencing related configuration for all rails and all devices on the bus. The main purpose of the report is to have a summary of the sequencing configuration of all the rails in 1 place, so that it is easier to compare and setup the system (which rail comes up first, depended on which rails, if fault occurs, which rails should be shut down, etc) => only the sequencing related configuration are saved to the report file.

    Currently, Fusion Digital Designer does not include GPO configuration in the report.