Hi,
As per the UCC2891 datasheet the OUT pin is capable of driving 2A.
However when i connect a resistive load of 10 Ohm between the OUT pin and GND to try source 1A current, the V_OUT(HIGH) drops down from 10V to nearly 5V. This indicates that the chip is capable of sourcing only (5V/10Ohm) = 0.5A current.
Can someone explain why the results are different from the datasheet specifications
Regards,
Kurian Polachan