8831.6332.5224.accessory.rarHello!
I am working on a power which is lmz12002 and lmr10520. Input 12V, lmz12002 provide 5V power, lmr10520 provide 3.3V power. when i used not analog 3.3V, 5V power have 400mv of burr and 3.3V power have 2v of burr. When i add analog 3.3V, 5V power have 2v of burr and 3.3V power will not work properly. Here attch my circuit and the output waveform. device packaging and pcb layout is according to the docimentation.Ask what's the problem.
Thank you!