I need to find out feasibilty of LM3481. For this I want power loss in IC.
Can I get power loss number and juction temprature at 125C ambient for following driving condition.
Vin=9 to 32 V.
Fsw=350KHz
LM3481 driving FET buk9616-75.
As per my calculation p_ic=Qg*Fsw*Vin
At vin=32V power loss is coming 0.47.
This power loss will give juction temp of 190C which will be far more than max. allowable junction temp.