Dear Sir/Madam,
I have an application where the LMZ34002 is required to power-on with the output disabled.
Logic level control is required to enable the output at a later stage.
Page 19 of the LMZ34002 datasheet shows a typical circuit to enable the output when low and disable the
output when high (opposite to my requirement). What would be the best option to achieve this requirement
from the least number of external parts.
Regards Grant