This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9248 monitoring FPGA temperature?

Other Parts Discussed in Thread: UCD9248

Hi

We are using the UCD9248 to control four single phase voltage rails, in a FPGA based system.

Since we have some temperature inputs left, we would like to monitor the temperature of the FPGA using the UCD9248, and turn off the power to the FPGA if it becomes too hot.

I don't see the functionality in the Fusion GUI, or in the controller datasheet.

Does anyone  know if this is possible?

It seems to be a relatively simple thing to implement into the controller?

 

Best regards

Bo Præstegaard Jensen, DHI