This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A4701 / accuracy of the Vref

Guru 20090 points
Hello,
 
Could you please let me know TPS7A4701 Vref accuracy?
Are below correct ?
 
Vref = 1.4V(typ)
Nominal Vref Accuracy: +/- 1% = 1.386V(min), 1.414V(max)
Overall Vref Accuracy: +/- 2.5% = 1.365V(min), 1.435V(max)
 
Best Regards,
Ryuji Asaka