Hi,
I Need 5V !a out of 20V - 30V, so I select the LM25011. Application note AN-1965 describes such circuit, ok, lets go.
After start testing, it turns out, that there is a Close relationship between Vin and Vou. The Output gets up to 5.35V, which makes the circuit useless.
I built two prototypes, so Errors by production are not very likely as both Shows exactly the same behavior.
Comparing the waveforms measured against the waveforms from the app note turns out significantly differences. My chip entered a hicup mode???
Any idea? I include the traces, Story and schematic.
Thanks a lot
Gerhard