Hello,
I am working towards a (non-host) smart battery with integrated charger, firstly using the bq20z65EVM and the BQ2476x EVM and have used SLUA533 as a guide. I would like to use the Input Current limit feature provided by the charger, but want to avoid having to use a host. I understand that the InputCurrentLimit register is volatile and defaults to 256mA when reset. Is it possible to have the coulomb counter configure the charger using a broadcast, (like the charge current and voltage), or will I need to add a host?
Thank you,
Jeremy.