Hello,
While doing a Point-of-Load design using the TPS40304, there seemed to be a discrepancy between the calculated phase margin and cut-off frequency of the control loop using the Compensation Calculator Tool (Rev. D Excel spreadsheet) and the Simple Switcher software. The design process was to first use the Power Stage Designer, then perform the compensation design using the Excel file and then finally input the entire circuit into the Simple Switcher tool. According to the Excel file, the bandwidth of the control loop was around 80kHz (which seems reasonable given the switching freq of 600kHz). When putting the same values into Simple Switcher, the bandwidth was only about 40kHz. The phase margin was also different but not as significant. Any ideas why there would be such a large difference between the two tools?
I have not tried various input/output parameters (designs) nor have I actually performed any control loop testing in the lab, but will be doing that this week. Any help in trying to understand why this would be very helpful as I would like some confidence in the compensation design in future designs.
Thanks!
Bill