Hello,
I am trying to design Buck converter using TPS62177DQCT. But across the datasheet they are suggesting maximum 10uH. Actually required current in our design is 80mA maximum. Input is 24V and output is 3.3V. With these specifications, if we are calculating for inductor value we are getting close to 180uH. Please let me know Do I need to follow the graphs given in datasheet and selected an inductor of value 10uH or do I need to follow calculations?
Also regarding the current rating for inductor, while choosing an inductor do I need to select inductor with current rating 2x or 3x times of the rate current of IC or 2x or 3x times the application maximum current? I want to use the following circuit in my design, shall I proceed with this or not?
Thanks,
Dhoresh.