Customer has used the TPS61161 with good success on the early samples they received. Their easy scale programming has not changed. The only change has been new silicon and they are claiming the FB pin ramps to and remains fixed at 600mV from power on.
The application is relatively straight forward, the input voltage is 5.1Volts. They are driving 6 series LED's at 20mA and are using a 10 ohm sense resistor.
When they used the sample silicon they were able to use Easy Scale as expected, the top side markings of the sample silicon used is:
XBZR
77K
D6HL
The production silicon FB pin immediately ramps to 600mV and they are unable to alter the voltage. Top side markings are:
BZR
82W
H7LR
Have there been any changes to the silicon or changes to the datasheet that we should be aware of? The version of datasheet we are working from is September 2008.
Thanks~!!!
Dale