Hello All,
I want to design a medical back-lit panel.
A medical product contains a back-lit panel. The panel lighting is an array of 9 sets of LED’s. These LED’s are arranged in three strings of 3 RGB LED’s as shown below:
The situation and requirements are:
1) A 6.0V power supply is available
2) The color of the backlight panel must be changeable to any arbitrary RGB combination via a serial communications interface (I2C, SPI or UART are all acceptable)
3) All three LED chains will always be lit the same color and the same brightness at any given time
Can you provide some insights as to which modules can be used in the design?
Thank you.
Regards
Ajay