This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25085 not bucking

Other Parts Discussed in Thread: LM25085A

We are testing a circuit designed with webench using the LM25085A. Vin 13.5-16V, Vout 12V, 5A. The circuit will pass through V when it is turned on but does not appear to be regulating. For example if we supply 14, 15 , or 16 V the output is the same as the input . Appreciate any suggestions. Thanks