Please see the attached file as wave form of the OUT pins.
Ryuji Asaka
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello, Asaka
what is the control mode customer select, voltage mode or peak current mode?
does customer add slope compensation if customer select peak current mode?
the jitter maybe caused by the transformer turns ratio is not exact between the primary and secondary windings of the power transformer.
Hello Asaka-san
You can try to measure the inductance of the two secondary windings of the transfromer. If the inductances between the two windings has big gap, there may have jitter on the output pins.
The jitter behavior is just peak curren mode control correcting the duty cycle to ensuring the transforme properly resets after every cycle.
Regards,
Yunsheng