Hi,
do you have any ideas how to create a power stage that is syncronizable from an external clock source, but if the ext clock disappears, the controller goes into disable mode.
The specs for the power stage are:
Vin: 24V
Vout: 5V, 1A max
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
do you have any ideas how to create a power stage that is syncronizable from an external clock source, but if the ext clock disappears, the controller goes into disable mode.
The specs for the power stage are:
Vin: 24V
Vout: 5V, 1A max
Most of our controllers will revert to a default clock frequency in the absence of an external clock signal. You will probably need to sense the clock externally and when it goes away have that circuit control the EN pin of the controller.
I don't have anything specific. So far as I know you are the first person looking for that solution. I think it would not be too difficult. The details would depend on your clock source and the type of controller you want to interface to.