Hi,
I try to design a DC/DC converter from 24V to 5V ( Imax =1A ) with Webench and SwitcherPro and i got two different schematic (attached .zip file). Which is the best? There are two difference point of work. If i try to impose the same resistor and capacitor value of Switcher Pro in Webench, Webench return different result of SwichePro, different point of work? Why, if the components are the same??? The pole, zero, phase margin would have to be the same!!!
Please help me in this choice. Thanks in advance.
Best regards.
Sandro