Hello
I had design based on LM5069 working properly up to now.
Basicallly is a DCDC converter from 48 to 24 (75W)
First stage of the power supply is the inrush controller based on LM5069-2
Current Limit 5A
Power Limit 25W.
My problem appears when input voltage switches from 48vdc to 56vdc once the power supply is working. The basically the LM5069 restarts and the power supply also does it during the insertion time (aprox 1 second)
The power supply input comes from 2 sources:
A 48VDC power supply (through a diode)
A 48V battery (which is around 56 volts on some circumstances.) through a relay.
The switching from one to another input is made by a relay (kind of UPS), so the step from 48 to 56 is practically instatntaneous and with no ramp (few microseconds).
I checked the 5 protections of the IC in order to find where the fails comes from
Current Limit
Power Limit
Circuit Breaker
UVLO
OVLO
The issue is that measuring the timer pin I can see that just inmediatly (2-3 microseconds) after 56 volts is present the insertion ramp starts and when reaches the 4 volts the circuit starts again and correctly.
(Also gate swithces off and the output of the mosfet and power good signal)
So if I am not wrong in any failure mode the fail ramp (which is much faster than the insertion one) should start and then a cycle of restart in case of fails remains. But I definetley see the insertion ramp.
I had no clear if OVLO and UVLO worked in the same way (fail ramp) so I disabled them by grounding OVLO and pulling up UVLO.
Same result.
I solved the problem with a serial inductance (330microH) in the input, but I would like to understand the behaviour.
Even more if the inductance is lower (100u) the behaviour is slightly different.
Just inmediatly after the 56 volts is present the gate switches off but timer pin remains low.
Quickly gate starts again and inrush works again limitng the I and rising Vo up to 56volts (30-40 miliseconds). No activity at the timer pin, but power good signal cycles (as Vds is higher than threshold) this time switching off my second stage.
Could you give me any idea why this restarting cycles could be activated at the LM5069?
Any advice would be welcomed.
Regards