Hi!
I have an external 350mA LED driver module (Vossloh-Schwabe ECXe 2350.037). I would like to use this module to drive 6×6 Seoul 5630 LED (100mA@3.2V). So basically, there are 6 strings of 6 LEDs with 59mA in each string.
But I need some cheap and effective current balancing/current limiting, so I have an idea: I will use a TL4242 in each string with 2.5Ohm R_REF (~70mA current limit).
Is that OK? I think, this solution more effective, than a simple NPN current mirror/sink, but I do not know, how operate six TL4242 in "paralel".
I saw other solutions (as LM3466, LM3464) but those did not meet the requirements, because this is a LED Tube application and the strings will far to each other.
Thanks!
PS.: Sorry for my bad English.