This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

20z65 LED states

Good afternoon,

I am using a 20z65 EVM to evaluate a prototype design.  The flash is configured for 5 LEDs.  Instead of having the LED indications be 0, 20, 40, 60 and 80% RSOC, I would like to customize these settings.  However, when I change the indicator settings in the flash, it does not work.  Regardless of my custom flash settings for charge and discharge LED indication, the LEDs only switch at equal 20% intervals.  Either this is a bug or I am missing something.  I can send you our .gg file if you like.  Other than that one issue, this 1p4s pack works fine.

--JP