I want the AME11865 (2000mAh) to update in the bq78pl116. In the chemistry selection table, the AME11865 is the 0206 chemical ID but in the bq wizard, the AME11865 is not include. Can I the 0206.chem with the AME11865?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Micou,
You can copy the 0206.chem file to your desktop, or some other location on our computer, and use the Chemistry Updater under Utilities>Add-ons in bqWizard to import the file. You can then go to File> Load Chemistry Data to import it into your device.
Tom
thank you for your reponse. I know the procedure maybe I want the 0206.chem file. Where have to I go to download the file?
You can search for Chemistry Updater on the TI website. Run this setup and the .cehm files should be placed in a directory similar to this one.
C:\Program Files (x86)\Texas Instruments\bq Evaluation Software\Plugins\Chemistry
I want update in the bq78pl116 for the ICR 18650-22P. I know, that the chemfile is 2002. Is it possible to copy this file into the subdirectory of the bqWizard and from where can I get it?
Thanks Karl
Karl,
The bqWizard program will copy the .chem file to the chemistry directory when you run the ChemistryUpdater routine located under the Utilities menu. You can place the 2002.chem file on your desktop to select it with the ChemistryUpdater.
Regards
Tom