Hello,
I have an application with a Xilinx Spartan 6 LX9 and I need to convert a 5v input supply to 3.3v (I/O and Aux) and 1.2v for the core of the FPGA. The application must use LDOs as it is in proximity of noise sensitive devices. I am considering the TPS7A7300 for both the 3.3v and 1.2v conversion.
If I use the 3.3V output of one LDO as the input to the 1.2V LDO, is there anything area I need to be concerned about?
Thanks for any help,
Rob Curtis