Hi,
I have two questions regarding the TPS55065:
1. Other than requiring a Vdriver > 5V at startup, is there a minimum load required for startup? If the load at startup is <50mA, does the device need to startup in low power mode?
2. What specs should the schottky diode have? The EVM does not follow the "Vf = 0.4V @1A, 125C" from the DS. What should the Vr (reverse voltage) spec be for this node - is 100V needed?
Thanks,
Adrian