This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65023 - Timing of switcher outputs



The customer has a question concerning the relative timing of the 3 switcher outputs VDCDC[1,2,3] in the datasheet. Data sheet allows  each output a Tstart and a Tramp. Tstart can be 140 to 200 uS and Tramp can be 400 to 1000 uS.

Are these times independent between the 3 switcher outputs? How well will they track, or not at all? That is, could DCDC1 start at 140 uS and DCDC3 start at 200 uS, or vice versa? Could DCDC1 ramp in 400 uS while DCDC2 ramps in 1000 uS?

 

Thanks