My situation:
When I apply power to the charger IC, the /PG indicates that power is good. The charger begins charging as indicated by the /CHG output. My battery charges either fully or at least it is almost full. But it continues to charge for 24 hours and probably longer. The /CHG output NEVER goes high.
My questions:
What are some possible causes?
Riset = 392ohms, so Iset = 1.25A. Iterm = 125mA. It is possible that my device is consuming more than125mA while charging. Could that cause /CHG to remain low? I was expecting that since the power is still connected, the battery would be fully charged, BGATE would turn off the external FET leaving the battery fully charged and proving power to the system directly through the SYS output.
The data sheet refers to "charging current" but what is that exactly or where can it be measured? Does it all flow out of the BAT or SYS terminals?
Thanks.