Other Parts Discussed in Thread: LM25118
I'm evaluating LM25118 for a buck-boost design with current ranging from 0.2A to 3.05A. The inductor selection in Workbench always return a 10uH inductor. However Equation 10 and 11 from datasheet results in an inductor of 75uH/42uH minimum. Also if I use a lower inductor the power supply will not operate in CCM and this behaviour is not explained in datasheet. Can I really use LM25118 for this design?
Vin: 6.54 to 32V
Vout: 12V
Iout: 0.2 to 3,05A
Regards,
Ana