This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Parallel Loaded Resonant Controller

Other Parts Discussed in Thread: LM25037

Hello,

I am a student working on implementing a Parallel Loaded Resonant Converter, but unlike the traditional version I am using a full bridge switching version as opposed to the usual half bridge. This requires similar switching signals to push-pull, and as such those are what I've been looking into using. 

My voltage inputs are 9-12 V, and as such the best option I've found yet is the LM25037. I would like to use others though if there are better choices, but so far the LM25037 is the best choice based on it's low voltage inputs. 

That being said:

1. Can anyone provide input to whether or not there are better, low voltage options? I've looked into several full-bridge/half-bridge driver ICs, but all that I've seen have been higher voltage than I can provide, without splitting the system into a primary and secondary stage. 

2. Could I request an evaluation board for the LM25037 to test against my hardware implementation? The datasheet for the LM25037 seems to imply that lower duty cycle is possible, but I'm having simulation issues implementing lower than 30% duty cycle. 

Thanks,

Nick