The V110 and V150 Tech reference for the bq20Z90/95 explain the "AFE OC Dsg Time" setting as follows:
Min Value = 0
Max Value = 0x0F
0x00 - 0x0f = sets the overvoltage trip delay between 1ms - 31ms in 1ms steps If the value varies by 30ms in 15 possible steps, (0x0F = 15[base 10]), then each step must be worth 2ms, not 1ms If I program-in a value of 0x04, I see a 9ms delay before the onset of AFE OC Dsg protection. So it looks like 2ms steps are the reality here. Anybody wanna gimme a buddy check? Regards, Michael A. Banak
http://eclectic-engineering.net