This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Your sch is ok. One suggestion: VPRG should be provided by an I/O port of MCU, just like other control signal(SIN, SCLK, etc), because you need program both GS register and DC register before turn on LED.
it's better to use another I/O port of MCU to control DCPRG, this will be convinient to switch between EEPROM and DC register when operation.
To cover green/blue LED forward voltage range, suggest use 4V for VCC. Consider only 30mA LED current, it's ok to connect cathod of red LED directly with OUTx pin. The power consumption inside 5940 is small.
Thanks