Good morning!!
I have 24V DC im my input, I did a converter with three outputs, +5V (1A), +18 (1A) e -18 (1A), I am using LM2576ADJ, my output -18V, how the diference betwen input and output is more than 40V, i did with HVT serieis with inverting buck boost mode, I need work with bateries in the input, i need the voltage with stabylity, because i use AD converter, my outputs isn´t good how I want, what kind of component it is better for this application? Or do you suggest other configuration?
Thanks.
Bento.