Hi, Kindly clarify the following points, regarding LM3447 data sheet:- 1) What is meant by Over 50:1 Dimming Range:
2) Angle Decoding Circuit & Dimming, Fig. 29 (Page No. 19,20 of LM3447 datasheet): It seems that below 30Deg phase angle, the graph saturates to below 0.3V, in this situation, what will happen for 0 Deg to 30Deg conduction angle. I think there is no change even if the power is dimmed below 30 Deg, then what will happen when customer needs to set the 5%, 15%, 25% intensities, will it not vary according to set value and when customer needs to set 0% will it not go to blackout? Pl clarify.
Regards Atul Bhakay