Hello,
I am using a boost converter controlled by an LM3478 to charge a pulse buffer. The buffer is rather large (1500uF). The buffer voltage can be adjusted from 20 to 40V. for this design I am trying to adjust the feedback behaviour.
I do not need a very fast or tight regulation, but I am hoping to get at least a bit better than I have now. I hope to get the following behaviour:
The buffer is charged to the set voltage level and then remains there until it is drained pulse-wise. A pulse will drain the buffer by at most 20%. It depends on the intensity and duration of the pulse. When the buffer is 10-20% below the set value I need the charger to give full power, otherwise proportionally less.
The current behaviour is that the buffer voltage will overshoot by quite a bit (estimate: 10%). Then the buffer drains slowly into the feedback network. If the voltage goes below the set value it will start to recharge and overshoot again. Now I have tried a number of settings for the compensation network, but I always get the same behaviour. I even tried to leave compensation pin open. I expected that this would result in a sort of bang-bang regulation, but again, the same behaviour.
Why does this happen? Is LM3478 also equiped with an internal compensation network? Are there other tricks I can use to get a more suitable behaviour?