Dear All,
Would you tell me about how to use on the board LP5521?
■There is a resistance near EN Pin in P22-Figure27 of the Datasheet.
Where is this resistance in the inside and the outside of the IC?
■In the case of those Pin disable,
do you recommend that customer perform pulling up of those Pin with 10kohms on their board?
■In the case of GPO disable,
do you recommend that customer perform open on their board?
■In the case of VDD=5V, do you recommend ChargePump disable?
Tsuguhiko Asai