This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The Output Capacitor for VDD2 on TPS65910A31A1

Guru 16800 points
Other Parts Discussed in Thread: AM3352

Hello,

I use TPS65910A31A1 for AM3352, and VDD2 of TPS65910A31A1 and CVDD_CORE of AM3352 are connected.
I have a question for the capacitance between two devices.

In datasheet of TPS65910A31A1, Filter capacitor Co(VDD2) is from 4uF to 12uF.
And in datasheet of AM3352, the decoupling capacitor of CVDD_CORE is 10.04uF.

So, I connect 10uF as the output capacitor of VDD2 and 10.08uF as the decoupling capacitor of CVDD_CORE.
The sum of two capacitances is 20.08uF.

Now, the combined capacity exceeds Filter capacitor Co(VDD2) of TPS65910A31A1.
Is this correct?
Should I set the combined capacity into Filter capacitor Co(VDD2) of TPS65910A31A1?

Best Regards.

Nomoto