This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM317M Temperature Range

I spec’d in LM317MDCYR  on a design I am working on.  The temperature range of the product is -35°C to +60°C. The link below is for the front page of the part.

 http://www.ti.com/product/lm317M

The temperature rating  for this part is called out as -40°C to 125°C under the "Parametric" and also the "sample and buy" sections, which is what I need for my application.  When selecting the part this is what I used.

However in the Data Sheet dated July 2006  it calls it out as 0°C to 125°C.   You need to order the part with a “Q” suffix to get a automotive temp. Datasheet link below:

http://www.ti.com/lit/ds/symlink/lm317m.pdf

But confusion comes in again when you go to Addendum-Page 1 of the datasheet. and the part is called out at the larger temp range.  The addendum is dated for 29-Jan-2014.

I have tested the part down to -35°C many times and the part functions correctly. 

So is the discrepancy of temps the case of the data sheet was not updated?  Just trying to see if I need to spec in another part.   Or what I have will work correctly?  I wasn't sure if there was a consolidation of parts and only the higher temp range is offered?