Hi,
Is it possible to use LM2585 with no load?
My configulation are as follows;
Input Voltage: 24V, Output Voltage: 48V, Load Current: 0A to 220mA
My concern is LM2585 works or not when load current down to 0A.
Thaks in advance
Hide
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is it possible to use LM2585 with no load?
My configulation are as follows;
Input Voltage: 24V, Output Voltage: 48V, Load Current: 0A to 220mA
My concern is LM2585 works or not when load current down to 0A.
Thaks in advance
Hide
Hi Hidetoshi,
Yes it will work with load currents down to no load.
Thanks,
Anston