Original Post by Avraka
Dear BIll
Regarding to the changes between 1.1.1 and 1.1.2, TPR #6 Coil test is added.
In 1.1.1, there are no issues. But 1.1.2 induce FOD and Temperature fails with the same TX board which is adopting BQ500212A.
In the beginning I used 3 COG + 1 X7R as a resonance cap. In this case, FOD is OK, but temperature is increasing.
If I use 4 COG, Temperature is OK. But It make a failure of FOD and TPR#6 Coil Test.
Making me know how to fix this issues would be appreciated.
Thanks