This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How do I balance 12 series connected supercapacitors?

Other Parts Discussed in Thread: BQ76940, BQ77910A

Is there an ic available from Texas for balancing 12 series connected supercapacitors?

I need to charge them a 4A maximum at a constant voltage of 30V (12 x 2.5V = 30V)

Thank you,

Stephan.

 

  • Hi Stephan,

    I would suggest looking at the bq76940 device. It can handle up to 15 cells, 48V and has the balancing feature. It is optimized for Li-ion though and is still in preview.the bq77910A handles just 10 cells, is a protector device but also does balancing

    -Onyx