Hi I need a small DCDC converter with secundair symmertical + and - DC output voltages in range of 13V to 16V.
I hope that I can achieve about 5% stability
The current drawn from he supply will be almost equal and vary from 20 to 60 mA max for each output.
The input voltage is not sure yet.. It could be 24DC but that voltage is not very stable and could vary +/- 10%
It is for the system not allowed to have an optocoupler in the feedback so I think I could use some primary side sensing?
Or maybe sense te input voltage and compensate for variations via the feedback of the IC.
The part I am thinking of is UCC2808 because I cannot use a flyback converter, but maybe there is a better choise now?
Cheers Bert