Can Rcsc on UCC28710 be left off if compensation not needed? The functional block diagram seems to indicate a yes, but the Detailed description doesn't clarify.
Also, the Irun parameter in Cdd equation is not defined in the definition of terms glossary, nor is it clearly described in the Vdd capacitance section text.
Similarly, it is not clarified if RLC can be a link (deleted) or has to be included. Only the pin function description alludes that it can be added, and hence inferred that it can be deleted/linked.