Via Webench, I got a design proposal with LM2673-adj to output 5V/2.5A from a supply ranged 10~26V. Webench suggested soft-start and Boost capacitor as 0.01uF, current limit resistor=9.79K, power inductor=33uH
I builded the circuit on a bread board and tested. The circuit was not performed as expected. It was 5.2V at no load. 3.5V at 5.6ohm load. Then the power inductor was changed from suggested 33uH to 10uH and boost cap to 0.02uF. Then 4.85V at 5.6ohm was achieved. But further test with 2.2ohm load got 3.02V. Decreased current limit resistor to 2.7K slightly increased the output to 3.3V at 2.2ohm load.
Please advice where should I look into to improve the circuit performance. Thanks for attention.