This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Vin:2.5V, Vout:7.5V, Iout:2A boost converter recommendation



Hi 

I'm looking for a part that can meet specification below:

Vin:2.5V

Vout:7.5V,

Iout: 2A

The current requirements is the output current not the switch current.

I tried searching the part using webench however there are no suitable part.

Can you please recommend a part that can meet the requirements?

Is is possible to meet the above requirements using step down DC-DC (SEPIC configuration)?

Kindly recommened a part that can meet the above requirements.

Thanks