Hello,
Here is a question about the design of TPS622x application, if the 3.3V Reg output what is th IC behavior if Vin became upper than Vout?
many thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS622x does not correspond to a proper part number. Please check which exact part you are asking about.
If you are asking about the TPS6122x boost converter, this wiki page has your answer: http://e2e.ti.com/support/power_management/non-isolated_dcdc/w/design_notes/1179.tps61220-performance-with-vin-near-vout.aspx
Oh yes you are perfectly right, there is a mistake in my question.
The IC is TPS6122x.
Thank you for the link.
If i understand, if the Vin is upper than 4,2V, the output is no longer regulated and vin is directly on Vout.
Is that right?
The problem is that in my application, Vin is mostly under 3.3V but sometimes can go to 5V.
Do you have an ic who have special feature to avoid this problem (like LTC3105 form linear technology)?
best regards,
A buck-boost converter would provide output regulation when Vin is above or below the setpoint. These are the TPS630xx devices (TPS63000, etc.).
But it sounds like you need a very low Vin boost IC. This would be the TPS61200. It has down mode, so Vout remains regulated when Vin goes above Vout. This is not the case with the TPS61220.