Hi,
I am using battery charger “BQ24103ARHLT” in one of my design. I’m using 2 cell Li-ion battery pack with nominal voltage of 7.4V with NTC. Supply input to the battery charger is 9V derived from “VSK-S5-9UA(CUI inc)” which is AC/DC converter with 9V as output voltage. The problem which I am facing is battery charger IC goes bad after few days. It happened in two boards and then I replaced IC. I am trying to find out the root cause for IC going bad. And more point is when I don’t connect NTC of battery to TS pin of IC, battery stops charging. Is it expected behavior? I have attached my schematic design. Need your help to find out root cause for IC going bad.