This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28550 - reading & writing Flash

Dear TI,

we use BQ28550 in a 1-Cell application.

I wrote a Visual Basic program to read out the Golden Flash an write it to an other device.

i use the function from BQ20z95 application notes.
Here is the save function. But this doesn't work. It makes a file, but there is no content (or the wrong content)

What is wrong?

Public Function saveDataFlashImagetoFile(ByVal sFilename As String, _
            sChipType As String) As Long
               
    'flash write
    'sChipType = "z80" or "z90"
    Dim iFileNumber As Integer
    Dim iNumberOfRows As Integer
    Dim iRow  As Integer
    Dim iIndex  As Integer
    Dim iLen As Integer
    Dim yRowData(32) As Byte
    Dim yDataFlashImage(&H700) As Byte
    Dim buf1$
    Dim arg As Long
    
    saveDataFlashImagetoFile = 0
    'directly from TI
    '//0x700 is the data flash size for bq8024-based devices (eg:bq20z80).
    '//     0x700/32 = 56 rows
    '//0x6C0 is the data flash size for bq8030-based devices (eg:bq20z90).
    '//     0x6C0/32 = 54 rows
    Select Case sChipType$
        Case "z70"
            iNumberOfRows% = &H6C0 / 32
        Case "z80"
            iNumberOfRows% = &H700 / 32
        Case "z90"
            iNumberOfRows% = &H6C0 / 32
        Case "z95"
            iNumberOfRows% = &H6C0 / 32
        Case "3060"
            iNumberOfRows% = &H400 / 32
        Case "28550"
            iNumberOfRows% = &H400 / 32
        Case Else
            GoTo saveDataFlashImage_error
    End Select
    
    '//PUT DEVICE INTO ROM MODE
    If putInRom <> 0 Then GoTo saveDataFlashImage_error
    DoDelay 0.01
    
     '//READ THE DATA FLASH ROW BY ROW
    For iRow% = 0 To iNumberOfRows% - 1
        
        '//Set the address for the row.  &H9 is the ROM mode command
        '//0x200 (512) is the row number where data flash starts
        '//Multiplication by 32 gives us the actual physical address where each row starts
        arg = (512 + iRow%) * 32
        If writeSMBusInteger(&H9, CInt(arg)) <> 0 Then GoTo saveDataFlashImage_error
        
        '//Read the row.  &HC is the ROM mode command.
        If ReadSMBusByteArray(&HC, yRowData, iLen) <> 0 Then GoTo saveDataFlashImage_error
        
        '//Copy dthis row into its place in a big byte array
        For iIndex% = 0 To 32 - 1
            yDataFlashImage((iRow% * 32) + iIndex%) = yRowData(iIndex%)
        Next iIndex%
 
    Next iRow%
    
    '//WRITE THE FLASH IMAGE TO THE FILE
    iFileNumber% = FreeFile
    Open sFilename$ For Binary Access Write As #iFileNumber%
    Put #iFileNumber%, , yDataFlashImage
    Close #iFileNumber%
    
    '//EXECUTE GG PROGRAM
    If executeGGProgram <> 0 Then GoTo saveDataFlashImage_error

Exit Function